Part Number: TPS25750
Other Parts Discussed in Thread: HD3SS6126,
Hi,
I just want to be sure my concept will work.
The USB TypeC should be used as a DFP to connect portable devices to a RF test equipment (which acts as Host, DFP). When the system is running, it should act as a source (5V/3A is enough).
When the system is in shutdown, it should be possible to charge the built-in battery (7S, 99Wh), therefore the controller should act as a Sink.
So my plan is:
- Configure the chip in safe mode for dead battery - it should get it's configuration from an EEPROM (I hope this way it can be configured and act as a Sink with up to 100W without the host booting)
- Configure only four PDOs (5V [seems to be required default], but skip the 9V and configure only 15V/3A, 20V/3A and 20V/5A (9V is too low and makes no sense for the buck boost charger)
and my questions are:
- What should be the default / preferred mode (sink or source?)
- Can I use the Event#61 (dp_dm_mux_enable_event) to control my USB3 Mux (HD3SS6126) depending on plug orientation (CC pins)? or should I use the Event#3 (Cable_Orientation_Event)?
- How to tell my charger to change it's current limits (based on 3A or 5A current contract) - take the Events#10...7 (SourcePDOxContract) and map them to IOs? or are there SinkPDOxContract Events?
- Charging the instrument works in dead battery mode (this might take hours). So clearing the bit using the Barrel_Jack_Event (Event#43) should work when the instrument is switched on?
any comments are welcome!
Thanks :)