This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: Gauge SOC is not changing

Part Number: BQ34Z100
Other Parts Discussed in Thread: GPCCHEM

Hi,

I'm using BQ34Z100PWR in a design. I have followed the steps mentioned in the datasheet regarding setting the various parameters for my battery pack, but the fuel gauge SOC doesn't change when I charge or discharge the battery multiple times. It always indicates 0 SOC and it doesn't change. Am I missing something? And how can I reset the chip to factory settings?

Here is a screenshot of the registers when the board is idle. I'm using this 6S LiFePO4 pack www.batteryspace.com/custom-lifepo4-18650-battery-19-2v-1-1ah-21-12wh-15a-rate.aspx

Appreciate any help here.

  • Hello Waseem, 

    Could you send over the .gg and log files? Additionally, what ChemID are you using and how was it matched? 

    To reset the chip to factory settings you will have to just program the srec file that you get when you download the device firmware from ti.com. 

    Regards, 

    Jonny Trevino. 

  • Hey Jonny,

    It turned out that the voltage on REGIN was dipping below limit and the chip was resetting, I have fixed that. But I've attached the .gg file and I would appreciate a quick look at it because I couldn't find a ChemID exactly matching my battery so I used the closest I could find in the list ChemID 0439. The log file was during the discharge portion of learning Qmax.

    Also, the app note SLUA334B mentions specific relax times (2 hours after charge and 5 hours after discharge). Are these strict values? or can I let the battery relax for longer or shorter time? maybe around 15 hours or 2 hours instead of 5.

    6076.FuelGauge.gg.csv

    Fri Sep 22 10:10:26 EDT 2023
    
    Device Name = bq34z100G1
    Firmware Version = 0_06
    
    
    Sample,DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags B,GridNumber,DoDatEOC,Qstart,TrueRC,TrueFCC,StateTime,DOD0PassedQ,DOD0Time,DOD0,QmaxDOD0,QmaxPassedQ,QmaxTime,LogRowTime(ms),LogStatus
    1,2023-09-22 10:10:31,4.887,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,885,SUCCESS
    2,2023-09-22 10:10:35,8.886,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1602,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,894,SUCCESS
    3,2023-09-22 10:10:39,12.884,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    4,2023-09-22 10:10:43,16.899,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    5,2023-09-22 10:10:47,20.916,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    6,2023-09-22 10:10:51,24.932,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    7,2023-09-22 10:10:55,28.930,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1602,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    8,2023-09-22 10:10:59,32.952,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,899,SUCCESS
    9,2023-09-22 10:11:03,36.951,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1602,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,885,SUCCESS
    10,2023-09-22 10:11:07,40.962,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    11,2023-09-22 10:11:11,44.964,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    12,2023-09-22 10:11:15,48.979,0x0006,0x0003,0,0,0,0,19452,0,-495,36.1,0,65535,0,-1605,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    13,2023-09-22 10:11:19,52.993,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,904,SUCCESS
    14,2023-09-22 10:11:23,57.027,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    15,2023-09-22 10:11:27,61.009,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    16,2023-09-22 10:11:31,65.009,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    17,2023-09-22 10:11:35,69.025,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    18,2023-09-22 10:11:39,73.024,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    19,2023-09-22 10:11:43,77.040,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    20,2023-09-22 10:11:47,81.055,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    21,2023-09-22 10:11:51,85.063,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,881,SUCCESS
    22,2023-09-22 10:11:55,89.071,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    23,2023-09-22 10:11:59,93.087,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    24,2023-09-22 10:12:03,97.105,0x0006,0x0003,0,0,0,0,19446,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    25,2023-09-22 10:12:07,101.109,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,883,SUCCESS
    26,2023-09-22 10:12:11,105.117,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    27,2023-09-22 10:12:15,109.152,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    28,2023-09-22 10:12:19,113.137,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    29,2023-09-22 10:12:23,117.168,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,902,SUCCESS
    30,2023-09-22 10:12:27,121.165,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1604,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    31,2023-09-22 10:12:31,125.167,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    32,2023-09-22 10:12:35,129.187,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    33,2023-09-22 10:12:39,133.198,0x0006,0x0003,0,0,0,0,19440,0,-495,36.1,0,65535,0,-1601,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,904,SUCCESS
    34,2023-09-22 10:12:43,137.196,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    35,2023-09-22 10:12:47,141.212,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    36,2023-09-22 10:12:51,145.229,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    37,2023-09-22 10:12:55,149.227,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    38,2023-09-22 10:12:59,153.246,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,885,SUCCESS
    39,2023-09-22 10:13:03,157.243,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    40,2023-09-22 10:13:07,161.242,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    41,2023-09-22 10:13:11,165.260,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    42,2023-09-22 10:13:15,169.292,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    43,2023-09-22 10:13:19,173.274,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    44,2023-09-22 10:13:23,177.305,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    45,2023-09-22 10:13:27,181.291,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    46,2023-09-22 10:13:31,185.321,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    47,2023-09-22 10:13:35,189.308,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    48,2023-09-22 10:13:39,193.339,0x0006,0x0003,0,0,0,0,19434,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    49,2023-09-22 10:13:43,197.337,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    50,2023-09-22 10:13:47,201.354,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    51,2023-09-22 10:13:51,205.351,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    52,2023-09-22 10:13:55,209.368,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    53,2023-09-22 10:13:59,213.388,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,900,SUCCESS
    54,2023-09-22 10:14:03,217.403,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,885,SUCCESS
    55,2023-09-22 10:14:07,221.383,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    56,2023-09-22 10:14:11,225.402,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    57,2023-09-22 10:14:15,229.402,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    58,2023-09-22 10:14:19,233.400,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    59,2023-09-22 10:14:23,237.417,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    60,2023-09-22 10:14:27,241.417,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    61,2023-09-22 10:14:31,245.447,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    62,2023-09-22 10:14:35,249.431,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    63,2023-09-22 10:14:39,253.448,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    64,2023-09-22 10:14:43,257.465,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.8,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    65,2023-09-22 10:14:47,261.446,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    66,2023-09-22 10:14:51,265.461,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    67,2023-09-22 10:14:55,269.479,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    68,2023-09-22 10:14:59,273.480,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    69,2023-09-22 10:15:03,277.495,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    70,2023-09-22 10:15:07,281.492,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    71,2023-09-22 10:15:11,285.508,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1600,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    72,2023-09-22 10:15:15,289.512,0x0006,0x0003,0,0,0,0,19428,0,-495,36.1,0,65535,0,-1603,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    73,2023-09-22 10:15:19,293.527,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    74,2023-09-22 10:15:23,297.523,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    75,2023-09-22 10:15:27,301.556,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    76,2023-09-22 10:15:32,305.571,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    77,2023-09-22 10:15:36,309.570,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    78,2023-09-22 10:15:40,313.571,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,921,SUCCESS
    79,2023-09-22 10:15:44,317.574,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    80,2023-09-22 10:15:48,321.586,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    81,2023-09-22 10:15:52,325.586,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    82,2023-09-22 10:15:56,329.606,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    83,2023-09-22 10:16:00,333.621,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    84,2023-09-22 10:16:04,337.619,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    85,2023-09-22 10:16:08,341.636,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    86,2023-09-22 10:16:12,345.634,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1599,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    87,2023-09-22 10:16:16,349.650,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    88,2023-09-22 10:16:20,353.648,0x0006,0x0003,0,0,0,0,19422,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    89,2023-09-22 10:16:24,357.669,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    90,2023-09-22 10:16:28,361.681,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1602,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    91,2023-09-22 10:16:32,365.664,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    92,2023-09-22 10:16:36,369.703,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,883,SUCCESS
    93,2023-09-22 10:16:40,373.696,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1599,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    94,2023-09-22 10:16:44,377.699,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1602,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    95,2023-09-22 10:16:48,381.712,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1602,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    96,2023-09-22 10:16:52,385.695,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1599,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    97,2023-09-22 10:16:56,389.728,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,1265,SUCCESS
    98,2023-09-22 10:17:03,396.650,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1602,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    99,2023-09-22 10:17:05,399.403,0x0006,0x0003,0,0,0,0,19416,0,-495,36.1,0,65535,0,-1599,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    100,2023-09-22 10:17:08,402.292,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    101,2023-09-22 10:17:12,405.781,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,883,SUCCESS
    102,2023-09-22 10:17:16,409.750,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    103,2023-09-22 10:17:20,413.762,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    104,2023-09-22 10:17:24,417.775,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,35.9,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    105,2023-09-22 10:17:28,421.792,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    106,2023-09-22 10:17:34,428.195,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    107,2023-09-22 10:17:37,430.742,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    108,2023-09-22 10:17:40,433.836,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    109,2023-09-22 10:17:44,437.826,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    110,2023-09-22 10:17:48,441.836,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    111,2023-09-22 10:17:52,445.840,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,901,SUCCESS
    112,2023-09-22 10:17:56,449.853,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    113,2023-09-22 10:18:00,453.871,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    114,2023-09-22 10:18:04,457.884,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    115,2023-09-22 10:18:08,461.900,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    116,2023-09-22 10:18:12,465.883,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    117,2023-09-22 10:18:16,469.930,0x0006,0x0003,0,0,0,0,19410,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,922,SUCCESS
    118,2023-09-22 10:18:20,473.901,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    119,2023-09-22 10:18:24,477.900,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    120,2023-09-22 10:18:28,481.980,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    121,2023-09-22 10:18:32,486.041,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,936,SUCCESS
    122,2023-09-22 10:18:36,489.961,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    123,2023-09-22 10:18:40,493.994,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    124,2023-09-22 10:18:44,497.946,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,922,SUCCESS
    125,2023-09-22 10:18:48,501.976,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    126,2023-09-22 10:18:52,505.993,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    127,2023-09-22 10:18:56,510.009,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1604,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    128,2023-09-22 10:19:00,513.979,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    129,2023-09-22 10:19:04,517.993,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    130,2023-09-22 10:19:08,522.040,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    131,2023-09-22 10:19:12,525.976,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    132,2023-09-22 10:19:16,530.009,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    133,2023-09-22 10:19:20,534.011,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    134,2023-09-22 10:19:24,538.025,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    135,2023-09-22 10:19:28,542.040,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    136,2023-09-22 10:19:32,546.058,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    137,2023-09-22 10:19:36,550.039,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    138,2023-09-22 10:19:40,554.039,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1598,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    139,2023-09-22 10:19:44,558.056,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    140,2023-09-22 10:19:48,562.071,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    141,2023-09-22 10:19:52,566.102,0x0006,0x0003,0,0,0,0,19404,0,-495,36.1,0,65535,0,-1601,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    142,2023-09-22 10:19:56,570.089,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    143,2023-09-22 10:20:00,574.102,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    144,2023-09-22 10:20:04,578.136,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    145,2023-09-22 10:20:08,582.121,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    146,2023-09-22 10:20:12,586.150,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    147,2023-09-22 10:20:16,590.137,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,885,SUCCESS
    148,2023-09-22 10:20:20,594.149,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    149,2023-09-22 10:20:24,598.164,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    150,2023-09-22 10:20:28,602.165,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    151,2023-09-22 10:20:32,606.164,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    152,2023-09-22 10:20:36,610.182,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    153,2023-09-22 10:20:40,614.215,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    154,2023-09-22 10:20:44,618.197,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    155,2023-09-22 10:20:48,622.197,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    156,2023-09-22 10:20:52,626.229,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    157,2023-09-22 10:20:56,630.230,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    158,2023-09-22 10:21:00,634.261,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    159,2023-09-22 10:21:04,638.258,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    160,2023-09-22 10:21:08,642.258,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    161,2023-09-22 10:21:12,646.296,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    162,2023-09-22 10:21:16,650.290,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    163,2023-09-22 10:21:20,654.289,0x0006,0x0003,0,0,0,0,19398,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    164,2023-09-22 10:21:24,658.292,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    165,2023-09-22 10:21:28,662.322,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    166,2023-09-22 10:21:32,666.322,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,921,SUCCESS
    167,2023-09-22 10:21:36,670.336,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    168,2023-09-22 10:21:40,674.322,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    169,2023-09-22 10:21:44,678.338,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    170,2023-09-22 10:21:48,682.370,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    171,2023-09-22 10:21:52,686.367,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    172,2023-09-22 10:21:56,690.370,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    173,2023-09-22 10:22:00,694.399,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    174,2023-09-22 10:22:04,698.383,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    175,2023-09-22 10:22:08,702.385,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    176,2023-09-22 10:22:12,706.399,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    177,2023-09-22 10:22:16,710.419,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1597,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    178,2023-09-22 10:22:20,714.437,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    179,2023-09-22 10:22:24,718.430,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    180,2023-09-22 10:22:28,722.457,0x0006,0x0003,0,0,0,0,19392,0,-495,36.1,0,65535,0,-1600,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,895,SUCCESS
    181,2023-09-22 10:22:32,726.464,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    182,2023-09-22 10:22:36,730.478,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.0,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    183,2023-09-22 10:22:40,734.481,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,904,SUCCESS
    184,2023-09-22 10:22:44,738.477,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    185,2023-09-22 10:22:48,742.498,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    186,2023-09-22 10:22:52,746.543,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1596,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,902,SUCCESS
    187,2023-09-22 10:22:56,750.515,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,882,SUCCESS
    188,2023-09-22 10:23:00,754.553,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    189,2023-09-22 10:23:04,758.527,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    190,2023-09-22 10:23:08,762.525,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    191,2023-09-22 10:23:12,766.542,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1596,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    192,2023-09-22 10:23:16,770.555,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    193,2023-09-22 10:23:21,774.572,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    194,2023-09-22 10:23:24,778.558,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    195,2023-09-22 10:23:29,782.571,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    196,2023-09-22 10:23:33,786.574,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    197,2023-09-22 10:23:37,790.586,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    198,2023-09-22 10:23:41,794.612,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,895,SUCCESS
    199,2023-09-22 10:23:45,798.603,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    200,2023-09-22 10:23:49,802.618,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    201,2023-09-22 10:23:53,806.620,0x0006,0x0003,0,0,0,0,19386,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    202,2023-09-22 10:23:57,810.634,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    203,2023-09-22 10:24:01,814.649,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    204,2023-09-22 10:24:05,818.655,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,883,SUCCESS
    205,2023-09-22 10:24:09,822.652,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    206,2023-09-22 10:24:13,826.667,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    207,2023-09-22 10:24:17,830.681,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,904,SUCCESS
    208,2023-09-22 10:24:21,834.697,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    209,2023-09-22 10:24:25,838.697,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1596,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    210,2023-09-22 10:24:29,842.699,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1596,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    211,2023-09-22 10:24:33,846.729,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    212,2023-09-22 10:24:37,850.731,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    213,2023-09-22 10:24:41,854.730,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    214,2023-09-22 10:24:45,858.744,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    215,2023-09-22 10:24:49,862.758,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    216,2023-09-22 10:24:53,866.759,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    217,2023-09-22 10:24:57,870.775,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    218,2023-09-22 10:25:01,874.793,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    219,2023-09-22 10:25:05,878.797,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,881,SUCCESS
    220,2023-09-22 10:25:09,882.806,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1596,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    221,2023-09-22 10:25:13,886.825,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,902,SUCCESS
    222,2023-09-22 10:25:17,890.824,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    223,2023-09-22 10:25:21,894.827,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,883,SUCCESS
    224,2023-09-22 10:25:25,898.837,0x0006,0x0003,0,0,0,0,19380,0,-495,36.1,0,65535,0,-1599,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    225,2023-09-22 10:25:29,902.841,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    226,2023-09-22 10:25:33,906.853,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    227,2023-09-22 10:25:37,910.853,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    228,2023-09-22 10:25:41,914.852,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    229,2023-09-22 10:25:45,918.868,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    230,2023-09-22 10:25:49,922.887,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    231,2023-09-22 10:25:53,926.886,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,902,SUCCESS
    232,2023-09-22 10:25:57,930.915,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    233,2023-09-22 10:26:01,934.914,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    234,2023-09-22 10:26:05,938.933,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    235,2023-09-22 10:26:09,942.933,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    236,2023-09-22 10:26:13,946.950,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    237,2023-09-22 10:26:17,950.961,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    238,2023-09-22 10:26:21,954.979,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    239,2023-09-22 10:26:25,958.993,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,904,SUCCESS
    240,2023-09-22 10:26:29,962.977,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    241,2023-09-22 10:26:33,966.997,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    242,2023-09-22 10:26:37,971.015,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,883,SUCCESS
    243,2023-09-22 10:26:41,975.028,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    244,2023-09-22 10:26:45,979.026,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    245,2023-09-22 10:26:49,983.045,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    246,2023-09-22 10:26:53,987.055,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    247,2023-09-22 10:26:57,991.058,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,886,SUCCESS
    248,2023-09-22 10:27:01,995.072,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    249,2023-09-22 10:27:05,999.086,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    250,2023-09-22 10:27:09,1003.103,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    251,2023-09-22 10:27:13,1007.118,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    252,2023-09-22 10:27:17,1011.118,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    253,2023-09-22 10:27:21,1015.118,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    254,2023-09-22 10:27:25,1019.133,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    255,2023-09-22 10:27:29,1023.137,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    256,2023-09-22 10:27:33,1027.148,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    257,2023-09-22 10:27:37,1031.166,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    258,2023-09-22 10:27:41,1035.168,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,887,SUCCESS
    259,2023-09-22 10:27:45,1039.198,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    260,2023-09-22 10:27:49,1043.227,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    261,2023-09-22 10:27:53,1047.227,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    262,2023-09-22 10:27:57,1051.305,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,906,SUCCESS
    263,2023-09-22 10:28:01,1055.211,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    264,2023-09-22 10:28:05,1059.245,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    265,2023-09-22 10:28:09,1063.211,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    266,2023-09-22 10:28:13,1067.228,0x0006,0x0003,0,0,0,0,19374,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    267,2023-09-22 10:28:17,1071.227,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    268,2023-09-22 10:28:21,1075.244,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    269,2023-09-22 10:28:25,1079.259,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    270,2023-09-22 10:28:29,1083.259,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,892,SUCCESS
    271,2023-09-22 10:28:33,1087.275,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    272,2023-09-22 10:28:37,1091.291,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    273,2023-09-22 10:28:41,1095.310,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,884,SUCCESS
    274,2023-09-22 10:28:45,1099.306,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,888,SUCCESS
    275,2023-09-22 10:28:49,1103.307,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,920,SUCCESS
    276,2023-09-22 10:28:53,1107.322,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,905,SUCCESS
    277,2023-09-22 10:28:57,1111.335,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    278,2023-09-22 10:29:01,1115.337,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    279,2023-09-22 10:29:05,1119.369,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1595,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    280,2023-09-22 10:29:09,1123.337,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    281,2023-09-22 10:29:13,1127.352,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,890,SUCCESS
    282,2023-09-22 10:29:17,1131.387,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,903,SUCCESS
    283,2023-09-22 10:29:21,1135.415,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,891,SUCCESS
    284,2023-09-22 10:29:25,1139.383,0x0006,0x0003,0,0,0,0,19368,0,-495,36.1,0,65535,0,-1598,36.1,2500,0,0,0,0x0961,0x0107,0xFFFF,8,98,13169,31284,12337,65328,896,-6,0,80,8307,17996,28233,889,SUCCESS
    

  • Hello Waseem, 

    • I recommend using the GPCChem tool to match the chemID, ideally you'll find a chemID with no more than 3% DOD error.
    • Regarding the relax time after charge and discharge, it is recommended to allow the battery to rest for 2 hours after charging and 5 hours after discharging. See sections 4.2.2 Relax for 5 Hours and 4.2.4 Relax for 2 Hours from How to Complete a Successful Learning Cycle for the bq28z610/bq78z100

    Regards, 

    Jonny T. 

  • Thanks for the help Jonny. I have used the GPCChem tool to find an appropriate ChemID, but the closest DoD error I got was 11.3%. To generate the csv file, I charged the battery to full, let it relax for 5 hours, discharged it, and let it relax for 5 hours. Attached is the GPC report I received, and the zip file I submitted to the tool3487.roomtemp_rel_dis_rel.zip.

    Chemistry ID selection tool, rev=2.54		
    		
    Configuration used in present fit:		
    ProcessingType = 2		
    NumCellSeries = 6		
    ElapsedTimeColumn=0		
    VoltageColumn = 1		
    CurrentColumn = 2		
    TemperatureColumn = 3		
    		
    Best chemical ID : 405	Best chemical ID max. deviation, % : 11.33	
    		
    		
    		
    Summary of all IDs with max. DOD deviation below 15%		
    		
    Chem ID	max DOD error, %	Max R deviation, ratio
    405	11.33	4.35
    481	12.26	0.69
    482	12.26	0.27
    6104	12.43	9.97
    4159	12.56	7.2
    410	12.63	0.43
    437	12.65	0.46
    426	12.69	8.44
    448	12.7	12.99
    427	12.81	0.41
    4110	13.14	0.23
    416	13.45	0.42
    459	13.57	10.68
    402	13.66	4.46
    414	13.74	8.92
    411	13.87	0.39
    400	13.96	0.4
    443	14	0.22
    462	14.09	0.57
    447	14.17	7.71
    4157	14.35	2.67
    425	14.38	10.14
    450	14.42	6.13
    451	14.43	8.95
    428	14.43	4.55
    461	14.44	4.58
    483	14.48	0.43
    432	14.57	0.5
    403	14.58	2.05
    484	14.61	0.53
    485	14.73	5.42
    487	14.73	5.45
    4138	14.92	1.33
    423	14.93	7.69
    491	14.96	12.16
    417	14.96	0.47
    		
    Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
    		
    		
    Selection of best generic ID for ROM based devices like bq274xx		
    		
    		
    Device / Family #1		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    354	bq27411-G1C: 4.35V LiCoO2	33.9
    3142	bq27421-G1D: 4.4V LiCoO2	38.4
    128	bq27421-G1A: 4.2V LiCoO2	39.13
    312	bq27421-G1B: 4.3V LiCoO2	87.74
    Best generic ID 354		
    Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
    		
    		
    Device / Family #2		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	33.9
    1202	bq27621: (default) 4.2V LiCoO2	34.08
    1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	38.36
    Best generic ID 354		
    Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
    		
    		
    Device / Family #3		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    3230	bq27426: (default) 4.35V LiCoO2	31.58
    1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	34.08
    3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	38.4
    Best generic ID 3230		
    Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
    		
    		
    Warning: Discharge rate is too high. High rate reduces ID detection accuracy	 10 hr rate is recomeended. Total discharge time is less than 5 hrs	 t_hrs=  3.57096805555556
    

  • Hello Waseem, 

    A DoD error of 11.3% is still to high to be very accurate. After looking at the data it looks like you are discharging at around C/4, I recommend discharging at a rate of C/10. The resting period of 5 hours should be fine. Please make sure you are charging the cell up to the recommended charging voltage stated on the battery pack. 

    Regards, 

    Jonny.