Hi,
I am using a LM3488 ic for converting from 24V to 5V in a motor driver circuit. The current limit of external power supply of 24V is set at 2A. The 24V is separately connected to motor driver also. Under some condition whethe motor draws large current the External power supply reaches current limit and drops to 4V. Under this condition for unknown reason. The LM3488 ic literally catches fire.
The circuit diagram of the LM3488 converter is exactly same as in the datasheet (except Rsn = 0.15 ohms) . The burnt image is shown below.