This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS628132MQWRWYRQ1 Instead of TPS57114CQRTERQ1

Hi,

Can I use TPS628132MQWRWYRQ1 instead of TPS57114CQRTERQ1(Existing) in my application?

My application requirements:

Vin: 4.5V

Fixed Vout : 1.8V

Max.Iout : 2A

Existing Operating switching Frequency: 1.66MHZ.

What Happens if I change switching frequency from 1.66 MHZ to 1.8MHZ or  2.25MHz with same requirements If I want to use TPS628132MQWRWYRQ1?