Part Number: BQ76952
Hi Expert,
During the initialization process, there must be an interval between writing subcommands. continuous writing will cause fail, the current setting is 1ms for the interval between two consecutive subcommands. The performance is normal. My customer wants to know is this time interval clearly mentioned in the datasheet?
here is what I reply to them:most command has a time to complete executation. Table 9-2. Command / Subcommand Operation Time
And BQ76952 has clock stretch function which can cause I2C communication fail when it can not response to the MCU.
Still, customer told me there is some commands are not covered by table 9-2, so they want to know that. Below is the command they provide to me:


Please kindly help on that.
BR
Emma