The purple waveform in the figure refers to the drive waveform provided by the UCC24612, while the yellow waveform refers to the voltage across the DS of the phase-shifted full-bridge secondary side MOSFET. Is this phenomenon due to the fact that the current at the end of freewheeling is too small, so the drive is turned off . Or is it due to the logic inside UCC24612 that is not suitable for phase-shifted full-bridge topology?