This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25622: Thermal shutdown behavior

Part Number: BQ25622

Hi team,

When BQ25622 get thermal shutdown, what's the exact behavior under this condition? Does Vsys still could get power from VBAT through BAT FET?  

Could you help comment on this?

Thanks and Best Regards,

Will

  • Hi Will, 

    We are checking on this and will get back to you in the next day or 2. 

    Best Regards,

    Garrett 

  • Hi Will, 

    When thermal shutdown occurs no matter whether the device is in buck mode, boost mode, or battery only mode the converter turns off and BATFET will be turned off to disconnect VSYS from BAT. In this scenario TSHUT_STAT bit in REG0x1F is set to 1b. 

    Then when IC temperature reduces BATFET is re-enabled and if device is in charge mode converter is re-enabled automatically as well. 

    This information will be included in the next revision of the datasheet. 

    Best Regards,

    Garrett