Other Parts Discussed in Thread: TPS22995H-Q1, TDA4VM, TPS22965-Q1
Hello TI,
Can you approve that one TPS6594-Q1 output GPO9 or GPO11 is capable to drive one TPS22995H-Q1 ON Pin (point-to-point connection with no additional leakage current)?
Background:
I am designing a circuit using the TPS6594-Q1 together with the TDA4VM, following SLVUC99A (PDN0-C).
This PDN recommends two TPS22965-Q1 Load Switches for supply of the 3.3 V I/O domains.
As dissimilarity aspects prevent the usage of TPS22965-Q1 in this application, TI suggests to use TPS22995H-Q1 as replacement.
The ON signals of the two load switches are driven by TPS6594-Q1 GPIO9 respectively GPIO11.
TPS6594-Q1 specifies 0.4V as the maximum low level output voltage at 3mA load current, there is no value given for lower current values.
TPS22995H-Q1 requires 0.35V as maximum low level input voltage at the ON pin.
Kind Regards, Peter