This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: GPIO Event #1: PlugEvent

Part Number: TPS25750

For some reason the SOM we are using needs a USB_OTG_VBUS Signal which normally is connected directly to VBUS at 5V systems.

Hence there are 5 to 20V on VBUS in this system I thought I can connect the GPIO Event#1 (PlugEvent) - "Asserted high when plug event (attatched state) has occured"

<- does this mean this GPIO is high as long as a USB-C cable is plugged in and VBUS switched on? Or only during the beginning until it is cleared.../whatever (The "has occurred" worries me)?