Other Parts Discussed in Thread: CSD19506KTT
Hi team,
Is there any 80V/100V NMOS with better specifications than CSD19536KTT? The SOA characteristics are required to be as good as possible, and the package can be larger than TO-263.
Nison
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Is there any 80V/100V NMOS with better specifications than CSD19536KTT? The SOA characteristics are required to be as good as possible, and the package can be larger than TO-263.
Nison
Hello Nison,
Thanks for the inquiry. The CSD19536KTT is our highest performance, 100V FET in D2PAK. The only other option would be the 80V, CSD19506KTT which has slightly lower on resistance (2.3mΩ max vs. 2.4mΩ max at VGS = 10V). However, the CSD19506KTT SOA performance is not as good as the CSD19536KTT. Both devices are also available in a leaded TO-220 package. Please let me know if you have any questions or need additional information.
Best Regards,
John Wallace
TI FET Applications