This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ66410: Capacity of internal input capacitors

Part Number: LMQ66410

Hi support team,

What is the capacity of each of the two internal input capacitors of LMQ664x0?

The diagram shows a series, but are you sure?

The internal bootstrap capacitor is 0.1μF, but is it the same capacity?

Regards,
Dice-K