This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25720: BQ25720RSNR : Battery NTC Pin

Part Number: BQ25720

Hi

We are using the battery charger (BQ25720RSN) in our laptop project. 

In this we are using three cell battery pack with nominal voltage of 11.1V. In this battery pack, there is one NTC pin which is used to measure the temperature of the battery pack. Normally battery charger IC has one dedicated pin where we can connect the NTC pin of battery pack to control the over temperature of battery pack due to charging. but this battery charger does not have any pin to connect to the NTC pin of battery pack to dis-connect charging due to over temperature.

So kindly let us know how we can use this NTC pin and where to connect.