What is the maximum sink current I(PD) of the TPS4811-Q1 when V(VS) = 25V to 55V and EN/UVLO is 0V and what is RPD in this case?
I need to be sure that the VGS of the external MOSFET is low when the TPS4811-Q1 is in low quiescent current mode and the MOSFET has high Gate leakage current.