Hi,
I am evaluating TPS25948EVM for my design.
As per datasheet TPS259480AYWP ( auto-rety enable ) should restart automatically after expiry of Trst which is 103 ms.
What i am observing is that the auto-rety is not functioning as expected.
For example
On the eval board U1 configured with current limit of 3A.
D3 turns on if the current drawn is more than 3A ( expected behaviour ).
But if the current drwan is decreased to a lower value , D3 keeps on till the current is decreaded 1.5A. ( as per my understadning D3 should turn off 103 ms after the over current condition is removed )
Request you to eloborate auto-rety functionality
Regards,
Anurag