I have had much difficulty trying to configure the TPS65987D with the user manuals and application notes found on the product page.
My application is to have the TPS65987D sink power from VBUS to PP_HV1 when it is not connected to power on PP_HV2 and source power to VBUS when power is available on PP_HV2. I have a 3.3v level signal coming into GPIO4 when power is present on PP_HV2. I create two configuration sets, and I have tried mapping GPIO4 to the "Barrel Jack Detect Event" and the "Port 0 Load App Config 1 Event". I do not see any changes when asserting/de-asserting the GPIO and while utilizing the debug mode to view the GPIO registers I also never see the state of the GPIO change
Attached is my .pjt file, any help would be greatly appreciated.