This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920: How to use a battery pack instead of separate battery cells?

Part Number: BQ76920
Other Parts Discussed in Thread: BQ34Z100-R2

Figure 9.1 of the technical sheet shows the connection of the battery cells, each one on a pin, can I use the 3 batteries inside a pack with this IC? How should I connect for this?

I see table 9.2 in the technical sheet but I don't understand if I need to use the 3 separate cells, or if I consider the pack as one, as my pack only provides me with 2 pins. How should I connect in this case?