This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z620: Golden image compatible with BQ28z610

Part Number: BQ28Z620
Other Parts Discussed in Thread: BQ28Z610, , BQSTUDIO

Hello,

If I have a golden image that was created using BQ28z610, can I use the same files for BQ28z620 or would I have to perform a new learning cycle?

Thanks,

Michael

  • Hello Michael,

    Learning cycles are performed so that gauges learn about the chemistry of the battery cell. The gauge learns the Qmax and Ra table. These values can be copied over.

    The only concern here is the memory mapping of both devices. They might have different registers. I suggest to download the BQ28z610 gg (configuration) file using BQstudio. Then, download the BQ28z620 gg file, and copy over the configurations from one to the other making sure they are the same registers. 

    Golden images (srec files) are not compatible. Meaning the BQ28z610's srec cannot be uploaded in the BQ28z620.

    Regards,
    Jose Couso

  • Hi Jose,

    Thanks for the reply! So once the values are copied over, we can just export a new srec for the bq28z620 correct?

    Thanks,

    Michael

  • Hi Michael,

    I suggest to calibrate the new device as well.

    As long as all modified registers are copied over, it should be ok. The challenge is making sure the register mapping is still the same. This is doable by doing bit to bit comparison in TRM and bqStudio.

    It is always good to do a sanity cycle check to make sure everything is working as expected.

    Regards,
    Jose Couso