Hi guys, I am designing a power mangement system using a BQ25792 for a 4s battery. I've attached my schematic below, its just a copy of the example schematic so hopefully everything is correct.
Here's a few notes about what you can't see on the schematic before I begin:
- I have a 10 kOhm thermistor connected to "Th1 and TH2" (Part number: TMP6131ELPGMQ1).
 - I ordered the wrong resistor for R2 so I've current got a 6.04k +-1% resistor on there and I am testing with a 2s battery for now.
 - I am providing 20v to VIN1.
 
I've assembled my prototype design and I'm at the testing stage currently. I'm trying to use the BQ chip without an i2c host but I can connect one for troubleshooting if neccessary. With the battery connected to "CELL4_OUT" I am seeing full battery voltage on the "VOUT1" pin which seems correct. When I supply power to "VIN1" however I see no change to the battery voltage even after a few minutes of having the power supply connected. The battery is only partially charged to about 7.7v so it should commence charging when there is power connected. There is currently no load on the "VOUT1" pin, I am just measuring voltage there. Without the battery connected if I connect power to "VIN1" I see about 3.5v on VOUT. I'm also seeing no activity from the LED connected between the STAT and REGN pins.
There is also an i2c current monitor on the board so the battery is connected through a 0.2ohm resistor before the BQ chip. Hopefully this isn't an issue!
Please let me know if you can see any obvious mistakes or what I should test to figure out what's going wrong. Everything is hand soldered with a hot air station so its possible something isn't making a good connection somewhere, but I have re-soldered the BQ chip several times and had the same result each time.
Cheers!