Other Parts Discussed in Thread: TPS563300,
Hello,
1) In Table 10.2 of datasheet, the recommended inductor values are only listed for switching frequency up to 1200KHz. Is there a reference value for 2200Khz?
And for 12V output, only 500kHz is listed. Is that because 1200Khz and above is not supported for 12V output?
2) Figure 10.8 shows the temperature is really high in maximum working condition. However i found this picture is exactly the same as TPS563300 (Fig. 8-7). Are they suppose to be the same?
Thank you.
/Roland