Hello,
I am working on a dc/dc flyback design. I have the device working well with a 16V output and 600V input. My only real issue is I am seeing some pulse width oscillation at lower power. I am using a type 2 compensator on the comp and feedback pins. I have the switching frequency set to 65KHz. I have included a Vds screenshot of the oscillation I am seeing.
Thanks,
Joe