Dear Team,
The recommended maximum output capacitor is 100uF in datasheet.
Our cutomer is using 112uF as the output capacitor.(10uFx11pcs+0.1uFx10pcs)
Do you have any concern?

Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
The recommended maximum output capacitor is 100uF in datasheet.
Our cutomer is using 112uF as the output capacitor.(10uFx11pcs+0.1uFx10pcs)
Do you have any concern?

Best Regards,
Hi Seijiro,
The effects due to DC and AC bias will likely bring down the effective capacitance to below 100uF. You can use an EVM to test a load transient with these capacitors installed to assess the stability, however I believe this is low risk and the design will probably be okay. If you want to conduct the test to be sure, follow this app note:
https://www.ti.com/lit/an/slva381b/slva381b.pdf
Thanks,
Stephen