This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS923653: Change of equations to the previous version

Part Number: TPS923653


Hi TI team,

I have one issues related to the TPS923653:

The equations on page 22 (section 9.2.1.2, equation 2,3,4,5) do not correspond, the values are modified and it is not really known how to select the components.
The values for the example could be Vin=12V, Vout=36V, ILED=1, FSW=1.5MHz, KIND=0.6, L=8.89uH, ILRIPPLE=.6, ILPeak=1.3, ILRMS=1.015.

It is not known which equations are correct.

Yo tengo una tension de 12, y necesito para mi diseño una salida en tension de 22 con una corriente de 350mA a una frecuencia de 400KHz y un Kind de .3.