I am building a circuit that uses LM5157 to boost the voltage from Vin: 5V to 12V and Vout: 13.5V (Iout=1A).
When the load characteristics were confirmed through actual measurements, the characteristics were as follows.
A voltage drop of about 0.5V was observed between no load and 1A load.
Is the above behavior normal for an IC?
Also, is it possible to eliminate the voltage drop during load by adjusting the peripheral circuits?
Input voltage: 12V fixed
| 負荷 | 出力電圧 | |
| 0 | mA | 13.530V |
| 100 | mA | 13.531V |
| 200 | mA | 13.531V |
| 300 | mA | 13.526V |
| 400 | mA | 13.421V |
| 500 | mA | 13.351V |
| 600 | mA | 13.253V |
| 700 | mA | 13.206V |
| 800 | mA | 13.117V |
| 900 | mA | 13.043V |
| 1000 | mA | 12.987V |