Dear Sir or madam,
We plan to use 3 TPS50601A-SP to provide (1.2V, 2.5V and 3.3V) power supply for a FPGA in a satellite.
The 3 TPS50601A-SP will normally work in external synchronization mode combined with Sequential Start-Up Sequence or Ratiometric Start-Up Sequence. We are not sure yet which start-up sequence to use.
The 3 TPS50601A-SP will get an external sync signal. I could read that the TPS50601A-SP will use its 500kHz internal switching frequency if the there is no sync during 20us. However, can you tell me:
- what will happen if the external sync is working again? I mean, will the TPS50601A-SP use the external sync as switching frequency again?
- will this sync scenario have an effect on the ratiometric or sequential configuration?
- if we use a ratiometric configuration, will the 3 TPS50601A-SP be switched off at the same time ?
- if we use a sequential configuration, will the 3 TPS50601A-SP be switched off in the reversed order of the start-up?
I am looking forward to hearing from you.
Best regards,
Axel Detrain