This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Billboard Event issue

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987,

Hi

We have a design with TPS65987D

Dual power role

UFP data role

DP alternate mode, DP receiver.

Application Customization tool: GUI Build Version: 6.1.4

Bootloader/application code version f707.10.10

The billboard event dosen't seem to work.

We want to use a GPIO to control an external USB billboard device to be enabled.

I configure a GPIO (for instance 12) as Direct mapped event to "Port 0 Billboard Event".

Connect a USB type A to USB-C cable.

We come up as Power Sink and Data Role UFP but with no PD negoiation and no DP Alternate mode.

But the GPIO 12 stays low.

I have also tried to enable the interrupts AMEnteredMode and AMEntryFail.

I do get AMEnteredMode interrupt when approriate but have never seen the AMEntryFail interrupt.

This looks a lot like the support case: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/836413/tps65988dj-tps65988dj-billboard-event-issue?keyMatch=TPS65987+BILLBOARD

I have also looked in the release notes for a different firmware: TPS65987_88_Firmware_Release_Notes_F907_14_14.pdf

Where they do mention a bug fix: Port does not assert Billboard event when AM entry fails

But the in the release notes for the firmware we are running: TPS65987_88_Firmware_Release_Notes_F707_10_10.pdf

There is no mention about billboard device issues.

Best regards,

Martin Bugge