This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: The Mosfets are not being fired by the IC appears to be in a shut down state

Part Number: LM5122

Design : 198 LM5122QMH/NOPB
LM5122QMH/NOPB 38V-55V to 65V @ 12A

The Voltage into the circuit is equal to the voltage out.

Vin+ 41 VDC

Vout = 41 VDC not 65 VDC

SS= 1.77V

Vcc= 7.6V

BST = 51V

FB= .75V

Web Bench Schematic 

lm5122 Schematic.pdf

My Schematic

Q500108 Schematic.pdf