Other Parts Discussed in Thread: BQ40Z80, BQ78350-R1A, BQ40Z50, BQ28Z610, BQSTUDIO
Dear TI team,
Good day!
We have a project using BQ40Z50-R4 for 3S1P polymer pack. Here we have some issues below and want to clarify how to update new settings every time we change.
(1). We have already got a Golden Image file following the TRM and just want to update some settings in data flash.
Could we use just export the updated gg file and import to other battery packs by using the procedure: import => Write all =>Read all(to double check)?
If yes, we have some trouble when we update the 45pcs sample but around 20pcs have error: CHGV wrong active when using correct charging voltage to charge 12.6V/1A (even lower 12V/1A also has the same problem) and can not be recovered staying in SAFE protection.
, and the power source was pulled at a high voltage 13V(around 0.4V) automatically after XCHG was active.
We check the all settings are all the same as other normal pack(which gg file should be completed updated) and the finally abnormal pack can be fixed by install the srec file.
(2).If we use the srec, should we need to calibrate the voltage, current, and temperature every time when update srec file?
(We found the voltage didn't change after update by srec file. Current sometimes has some tolerance, Temperature by TI default seems be within acceptable tolerance range always without calibration)
(3).Is there any step need to be careful when install gg file and srec?
We found that different gauge IC we use (BQ28Z610, BQ40Z50, BQ40Z80, BQ78350-R1A) has different situation when update gg file, such as waiting time, data flash need repeat importing process more than one time.
Is there any reason or any related factors?
Your advices will be very appreciated.
Thanks and best regards,
James