This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

run time error '6' - overflow

 I am using bqEASY to program bq20z95 & above error is generated by entering following values:

1. No of cells in series - 4

2. no of cells in parallel  - 15

3. short circuit protection during charging - 15 AMP

4. Max steady state discharge current - 20000 mA

5.Peak short term discharge current -25000 mA

6. Short circuit detection during discharge- 30A

Rest of parameters are entered as I had done in my earlier projects & showed no error.I think this is due to large current values.

Please confirm me is this error is due to large current values & what is the solution for this. And if this error is due to large current values then what are the threshold values in above case.