This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: OCD1 Threshold value multiplier.

Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO

In TRM, the OCD1 Threshold multiple is written 2mV. But BQSTUDIO doesn't show 2mV please clarify. 

  • Hi Nick,

    The setting can be changed in increments of 2mV, hence the unit being 2mV in the TRM. However, this isn't as user-friendly as using 1mV for the unit, so to make it easier to read what value the setting actually is, bqStudio translates the setting to 1mV units.

    For example, if the setting was 164mV, it could be confusing to see that in bqStudio as 82 * 2mV.

    Regards,

    Max Verboncoeur