This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: Used to share current in oring application

Part Number: UCC39002
Other Parts Discussed in Thread: TPS2410,

Hi Team,

My customer uses TPS2410 to implement oring solution. However, it was found that when there is a voltage difference between two power modules, then only one module is working, when the working power module is unplugged, there will be a voltage drop (switching delay) at the load side. I want to use UCC39002 to make two modules power the load at the same time, so that when one of the modules is unplugged, there will be no voltage drop at the load side. Could you please check if this is possible?

Regards,
Hailiang