3 sting
12-18V INPUT
Sting 1= 18V 80mA
Sting 2 = 18V 80mA
Sting 3 = 16.8V 10mA
Individual PWM control OR I2C
Fault Detection
For our application, we will need to drive 2 stings of LEDs at 18v 87mA, and a single string of LEDs at 16.8V 10mA. We will not be driving stings (1,2) at the same time as 3 (STING 1-2 ON/STING 3 OFF) (STING 1-2 OFF/STING 3 ON)
We have 18V or 12V available to power Driver.
Do you have an LED driver that could work/is recommended for our application?