This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: IOTG_regulation and Charger_Control_1 settings

Part Number: BQ25798

Hi, 

We are using the BQ25798EVM and the online TI Charger GUI.  The datasheet has Bit 7 of register 0x0D as 0b 2 hrs (default) and 1b as 0.5 hrs.  The TI Charger GUI has it the opposite.  I'm assuming the datasheet takes precedence?  Just need to verify.  
The datasheet has bits 5:4 of register 0x10 as 00b 26V, 01b 22V, 10b 12V and 11b 7V.  The TI Charger GUI has register 0x10 as 00b 26V, 01b 18V, 10b 12V and 11b 7V.  For the 10b setting I'm assuming the datasheet takes precedence?  Just need to verify.

Thanks, 

Paul