When TPS65981 External HV Power Switch is configured as a Sink With RSENSE, the Rsense is used to provide current measurement and current limit. If there's a short time big value inrush current, but I don't want to trigger this over current protection of TPS65981. Can I configure this feature in the "TPS6598x application Customization Tool"? For example add some delay time to ignore short time inrush current. I noticed that there's something like "external power path over-current timeout ", is that for this purpose? I have tried to configure the time to maximum value 81.92ms in the Tool software, but the over current still triggers.
Can this current limit feature be shut off completely?