Hi,
I am unable to save UCC25600 simulations in Pspice for TI tool. It's giving the below error message.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am unable to save UCC25600 simulations in Pspice for TI tool. It's giving the below error message.
Hi Navaneethrj,
I did a search on ORCAP-1682 and the only hit I got was from 2011. An issue with the name being in lower case, but that was supposedly fixed.
I was able to pull the reference design for this part and run the transient without a problem.
Can you confirm your version? Go to Help, About and you should see PSpice for TI, PSpice_TI, 17.4-2023 S009
Did you first run the reference design? If that works, it might give us a clue as to what's going on.
David
Hello David,
My version is 17.4-2023 S009 SPB 64 bit Edition.
Yes, i can run the reference design and it is working.
The ORCAP-1151 error can be resolved as follows:
This is because the active simulation profile is not configured to the schematic you are trying to simulate. Please right click on the correct simulation profile and make it active.
David