Hi
Is there a duty limit for TPS28225 as well?
Ask if there is a possible min/max value.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Is there a duty limit for TPS28225 as well?
Ask if there is a possible min/max value.
Thanks
Hi David,
The part does not have an inherent limit to duty cycle; it can hold UGATE on or off indefinitely as long as its set up properly for that.
The bootstrap supply for the high side does impose a duty cycle limit because it requires LGATE to turn on occasionally to recharge. It is usually possible to reach very high duty cycles of >98% using the bootstrap circuit, but it must be designed well.
It can hold off in DC, but small pulses can be an issue. There should be no pulses under 30ns in width. The duty cycle that corresponds to depends on the Fsw of the system so I can't give a number.
Thanks,
Alex M.