This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62A01: question

Part Number: TPS62A01

Hello Experts,

My customer has question as follows. Would you answer it, please?
1. output capacitor
The datasheet mentioned that recommended output capacitor value is 22uF x 2pcs when Vout is 0.6V< Vout< 1.2V. If customer chooses 47uF x 1pcs, is there any limitation?

2. feedforward capacitor
The datasheet recommend 120pF, in case of Vout=1.8V. If customer set Vout=1.15V, how to decide a feedforward capacitor value?

3. IHC(OC)
Would you tell IHC(OC) max spec, please?

Best Regards,
Fujiwara