HI Dear,
The customer needs to obtain intrinsic safety certification for underground related equipment. The certification requires that the total capacitance in the circuit cannot exceed a certain value. May I ask if there is a bypass capacitor that can achieve a DC-DC chip of 1uF, with an input voltage of around 22V and an output requirement of around 1-2A