This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5158: for output 54v design

Part Number: LM5158

Hi Sir,

we have new design specification as below, if use boost Topology,  can LM5158 be design with follow specification?

Input=40V~54V

Output=54V/420mA = 22.68W

also we want to know the efficiency curve below,  could it be provide?

vin 40v , Vout 54v/ 0.42A

vin 48v, Vout 54v/ 0.42A

vin 54v, Vout 54v/ 0.42A

if this SPEC does not apply to the LM5158, any suggest solution?