This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR54410: The selection of the Capacitor for the LMR54410

Guru 12785 points
Part Number: LMR54410


Hi,

Q1.
I have a question regarding the selection of the input capacitor Cin for the LMR54410FDBVR. The datasheet states that the general recommended value for the high-frequency decoupling capacitor Cin is 2.2 μF or more, but is there any problem even if this value is less than 2.2uF? Due to the DC characteristics and withstand voltage rating of the Ceracon, the selected Ceracon may not be 2.2 uF or higher.
 
Q2.
Similar to Q1, the datasheet states that a capacitor with a value of 0.1 μF should be placed for high-frequency filtering, but to what extent can this value also vary?

Background to the question.
Since the capacitor questioned in Q1 and Q2 is a filter for high frequencies, I am wondering whether there is any problem with a design using a Ceracon with an ESR on the order of several mΩ around 1.1 kHz, the frequency of the switching regulator, even if the recommended Ceracon capacitance is not used.

Thanks,

Conor