Hi
I have a query need your help. According to the datasheet how to calculate the current error.
Please provide calculation formulate.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Star,
Assuming we ignore non-linearity and offset. The current error would be determined by the gain error.
Datasheet gives a worst-case gain error of 1.5% of the full scale range of the coulomb counter. the full range is -270-mV to 270-mV. So, 1.5% of this range would correspond to ~4-mV of gain error across the whole range. This would be the error at the edges of the voltage range of the coulomb counter, so at ~270-mV.
Let's assume that there is a 2000-mA current flowing through, if we assume the worst gain error is 1.5%, this means that the measurement could be read as 2030-mA. Although this depends on the sense resistor used. The current error due to gain will never be more than 1.5%.
Offset and INL errors are given with respect to LSB's. Which is given as 8.44-uV per LSB.
Best Regards,
Luis Hernandez Salomon