Other Parts Discussed in Thread: TPSM63610,
Hello Team,
according to below table we recommend Fsw = 500kHz to 1.4MHz for Vout=5V (I guess the Fsw to Vout=9V is wrong?)
The max duty cycle at Fsw = 1.85MHz is specified with 87% typically:
For the given application the duty cycle = 5V/6V = 83.3%. Is that supported at Fsw=1MHz?
Is the duty cycle dependent on switching frequency?
Thank you and Best Regards, Hans