Other Parts Discussed in Thread: TPS54140
Hi,
Using webench to simulate TPS54340, the conditions are shown in the figure, but there is a problem that cannot be simulated. What is the reason?
Customer input is around 22V, output requires 5V 2A.
According to the above requirements, can the bypass capacitor of TPS54140 input end be used for 1uF?