Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200D2EVM: How to evaluate the loop response

Part Number: TPS92200D2EVM

Dear TI team

 

I have a question related to the content of the thread below.

I didn't get an answer in the previous thread, so I asked again.

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1220624/tps92200d2evm-how-to-evaluate-the-loop-response/4611848?tisearch=e2e-sitesearch&keymatch=%252525252525252520user%25252525252525253A449265#4611848

 

Please tell us how to evaluate the loop response with the EVM of this IC.

I am aware that I should evaluate by removing R7 (0Ω) on the EVM and instead populating R5 (49.9Ω) for signal injection. Is this perception correct?

 

We also recognize that there are multiple measurement methods (such as using FRA).

If you have detailed documentation or notes on evaluation, I would appreciate it if you could share them.

 

Best Regards,

Taroimo

  • Hi Taroimo,

    Sorry for missing the previous thread.

    I am aware that I should evaluate by removing R7 (0Ω) on the EVM and instead populating R5 (49.9Ω) for signal injection. Is this perception correct?

    Yes. You are correct.

    You can use a frequency response analyzer to do the measurement. You can apply the stimulus signal through an injection transformer to the TP6 and TP5 on the TPS92200D2EVM. The output signal can be measured from TP5 on the EVM. The input signal can be measure from TP6 on the EVM. The loop response can be calculated from the measured output and input signal.

    Best Regards,

    Steven