This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2372: TPS2372

Part Number: TPS2372

I have a question regarding UPOE support on TPS2372-3 PD.  with single PD device configured as class 4 (both class A and B resistors are set at 63.4 ohms) device and no LLDP connected to UPOE switch,  what will happen if UPOE PSE is forced to source power on all 4 pairs.  How would UPOE switch will see PD.  as two class 4 devices ?  or will it see it as a single class 4 device?