I have a question regarding UPOE support on TPS2372-3 PD. with single PD device configured as class 4 (both class A and B resistors are set at 63.4 ohms) device and no LLDP connected to UPOE switch, what will happen if UPOE PSE is forced to source power on all 4 pairs. How would UPOE switch will see PD. as two class 4 devices ? or will it see it as a single class 4 device?