Other Parts Discussed in Thread: TPS25982, , BQ24618
I have copied the application schematic from the datasheet and added a custom PCB. I have an intermittent problem where at some point Q5, from the datasheet and the IC will explode when the battery is inserted. It doesn't happen every time. I've had these boards for a little over a week now and during that time 3 of 5 have popped. Since it is only the IC and Q5 that are damaged I assume that means that the chip is turning on LODRV for some reason when it first gets connected and pulling large amounts of current through Q5. The IC failure only happens when the battery is 1st inserted. So far, if the failure doesn't happen on battery insert, then the board runs fine.
Is this a known issue?
Although not in the datasheet, would adding a pull down to LODRV prevent it from turning on when the battery is inserted?
You can see Q5 has internal metal exposed and hole burned through U1. Schematic attached incase my I'm missing some configuration error compared to the datasheet.