This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SG3524: SG3524 vs DRV8251 of Motor Design

Part Number: SG3524
Other Parts Discussed in Thread: DRV8251,

hi ,

I want to design a compressor that conforms to two different architectures

item1 have 3pin input,The middle tap of the coil is connected to 12v

item2 have 2pin input,

I want to use DRV8251 to control item1,it's can't normal work,

Is there an ic solution that can be shared by both?

Or do you have any suggestions on how to package SG3524 and MOSFET together?

1.

2.