This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM63610-Q1: Bode plot measurement

Part Number: LM63610-Q1

Hello,
What is the setup in order to measure the Bode plot? 

  • Hi Jason,

    You need to have a loop test resistor(just refer to R1, the value is about 49.9ohm). Then use a loop analyzer to measure. The red terminal for signal injection is connected to Vo, and the black terminal is connected to Vloop. The A terminal for signal detection is connected to Vloop, and the B terminal is connected to Vo. Thanks.

    Aurora