This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51430: LMR51430 to replace TPS563252

Part Number: LMR51430
Other Parts Discussed in Thread: TPS563252,

Hi team,

Schneider encountered a problem in IC selection and would like to inquire whether LMR51430 can be used instead of TPS563252.

The application is to power radio frequency devices, which has relatively high requirements on ripple and response speed.

Input 10V, output 3.8V, transient is responsible for 0.1A to 2A, Drop is not lower than 3.3V, recovery time is about 4ms

The main reason is that LMR51430 DS does not indicate that it can be used in radio frequency applications, so I am not sure, could you help check for this?

...

Thanks

Lillian