Other Parts Discussed in Thread: LM25149, LM5149-Q1EVM-400, PMP20804
LM25149-Q1 Is this part support for 40A load?
My input is 24VDC and Output is 12V/40A is this the right part to use.
if not suitable then suggest the part which can be best suited for my application.
Requirement is:
Input is 24VDC and Output is 12V/40A
and the part must have ultra-low IQ and integrated active EMI filter.